eMMC memory to KINETIS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eMMC memory to KINETIS

2,858 Views
goranigic
Contributor II

Is there any application note how to connect eMMC to KINETIS (K65)?

eMMC.png

4 Replies

2,467 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please check below eMMC interface schematics example. Thee are no dedicated lines for card detection [CD] and write protection [WP], which must be implemented using GPIOs, also; all the lines must have a 4.7K pull up resistor tied to a VDD=3.3V.

eMMC-Kinetis.png

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,467 Views
goranigic
Contributor II

Hi Hui,

Thanks,

Just a quick question

the SSP0_Interface is available in K65?

Goran

0 Kudos
Reply

2,467 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Goran,

K65 doesn't have dedicated SSP interface (Synchronous Serial Port), while it provides SPI/I2C/I2S interface.

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,467 Views
goranigic
Contributor II

Is it possible to use SDHC connections to connect to the eMMC?

Thanks,

Goran

0 Kudos
Reply