d4dlcdhw_template_ID

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

d4dlcdhw_template_ID

1,957 Views
ankurchauhan123
Contributor I

Hi,

I'm using TWR-K70 kit with TWR-LCD module.

I'm trying to use D4D libraries.

I'm getting the following error:

Undefined Reference to d4dlcdhw_template_ID

in the following line :

D4D_LLD_LCD_HW.D4DLCDHW_WriteData(win_cur_addr, value);

what could be the resaon???

Regards

Ankur

Tags (1)
0 Kudos
Reply
2 Replies

1,903 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

What IDE are you using? You have a working project here: https://github.com/Gargy007/eGUI

If the IDE is different, be sure you're using the right configuration of the library (low level drivers).

Luis

0 Kudos
Reply

1,903 Views
ankurchauhan
Contributor I

Hi Luis,

Thanks for reply.

I'm using CW 10.6.4

0 Kudos
Reply