controlling UART ISR directly with (bypassing) MQX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

controlling UART ISR directly with (bypassing) MQX

Jump to solution
3,478 Views
MichaelDavid
Contributor III

 

I'm trying to configure a UART ISR.

I using MQX, but here I want to control the ISR directly.

The ISR doesn’t work when I start writing. (after sending one byte It doesn’t enter to the ISR )

Can You see if there is something missing in my configuration.

Michael David.

 

Here is my UART Configuration:

 

void Uart_InitUart(void)

{

      uint_16 ubd,temp0,temp1,brfa;

      uint_32 sysclk = BSP_SYSTEM_CLOCK, baud0 = 57600;

      //UART configuration

      SIM_SCGC4 |= (SIM_SCGC4_UART0_MASK);

     

      PORTA_PCR14 = PORT_PCR_MUX(3);      //TX 0

      PORTA_PCR15 = PORT_PCR_MUX(3);      //RX 0

     

      UART_C2_REG(UART0_BASE_PTR) &= ~(UART_C2_TE_MASK | UART_C2_RE_MASK);

      /* Configure the UART for 8-bit mode, no parity */

      /* We need all default settings, so entire register is cleared */

      UART_C1_REG(UART0_BASE_PTR) = 0;

      /* Calculate baud settings */

      ubd = (uint_16)((sysclk*1000)/(baud0 * 16));      

      /* Save off the current value of the UARTx_BDH except for the SBR */

      temp0 = UART_BDH_REG(UART0_BASE_PTR) & ~(UART_BDH_SBR(0x1F));

      UART_BDH_REG(UART0_BASE_PTR) = temp0 |  UART_BDH_SBR(((ubd & 0x1F00) >> 8));

      UART_BDL_REG(UART0_BASE_PTR) = (uint_8)(ubd & UART_BDL_SBR_MASK);

      /* Determine if a fractional divider is needed to get closer to the baud rate */

      brfa = (((sysclk*32000)/(baud0 * 16)) - (ubd * 32));

     

      /* Save off the current value of the UARTx_C4 register except for the BRFA */

      temp0 = UART_C4_REG(UART0_BASE_PTR) & ~(UART_C4_BRFA(0x1F));

      UART_C4_REG(UART0_BASE_PTR) = temp0 |  UART_C4_BRFA(brfa);

      /* Enable receiver */

      UART_C2_REG(UART0_BASE_PTR) |= ( UART_C2_RE_MASK | UART_C2_TE_MASK);

      // configure ISR  - UART 0 IRQ - 45

      NVICICPR1 |= (1<<13); //45 MOD 32

      NVICISER1 |= (1<<13);

      NVICIP45 = 0x30;        // priority 3. out of 15

     

      Isr_InitIsr(INT_UART0_RX_TX, Uart_RxTx0_Isr);

}

 

Here is the Isr_InitIsr function:

 

void Isr_InitIsr(_mqx_uint isr, void (_CODE_PTR_ isr_func)(pointer))

{

      MY_ISR_STRUCT_PTR  isr_ptr;

     

      isr_ptr = _mem_alloc_zero((_mem_size)sizeof(MY_ISR_STRUCT));

     

      isr_ptr->TICK_COUNT   = 0;

      isr_ptr->OLD_ISR_DATA = _int_get_isr_data(isr);

      isr_ptr->OLD_ISR      = _int_get_isr(isr);

     

      _int_install_isr(isr, isr_func, isr_ptr);

}

 

0 Kudos
Reply
1 Solution
2,315 Views
MichaelDavid
Contributor III

here is the solution:

void Uart_InitUart(void){ uint_32 ubd0,ubd1,ubd3,temp0,temp1,temp3,brfa; uint_32 sysclk = BSP_SYSTEM_CLOCK,busclk = BSP_BUS_CLOCK,  baud0 = 115200, baud13 = 57600; //UART configuration SIM_SCGC4 |= (SIM_SCGC4_UART0_MASK | SIM_SCGC4_UART1_MASK | SIM_SCGC4_UART3_MASK);  PORTA_PCR14 = PORT_PCR_MUX(3);      //TX 0  PORTA_PCR15 = PORT_PCR_MUX(3);      //RX 0  PORTC_PCR4  = PORT_PCR_MUX(3);      //TX 1  PORTC_PCR3  = PORT_PCR_MUX(3);      //RX 1  PORTB_PCR11 = PORT_PCR_MUX(3);      //TX 3  PORTB_PCR10 = PORT_PCR_MUX(3);      //RX 3  UART_C2_REG(UART0_BASE_PTR) &= ~(UART_C2_TE_MASK | UART_C2_RE_MASK); UART_C2_REG(UART1_BASE_PTR) &= ~(UART_C2_TE_MASK | UART_C2_RE_MASK); UART_C2_REG(UART3_BASE_PTR) &= ~(UART_C2_TE_MASK | UART_C2_RE_MASK); /* Configure the UART for 8-bit mode, no parity */ /* We need all default settings, so entire register is cleared */ UART_C1_REG(UART0_BASE_PTR) = 0; UART_C1_REG(UART1_BASE_PTR) = 0; UART_C1_REG(UART3_BASE_PTR) = 0; /* Calculate baud settings */ //ubd = (uint_32)((sysclk*1000)/(baud0 * 16)); ubd0 = (sysclk + 8 * baud0)/(16 * baud0); ubd1 = (sysclk + 8 * baud13)/(16 * baud13); ubd3 = (busclk + 8 * baud13)/(16 * baud13);   /* Save off the current value of the UARTx_BDH except for the SBR */ temp0 = UART_BDH_REG(UART0_BASE_PTR) & ~(UART_BDH_SBR(0x1F)); temp1 = UART_BDH_REG(UART1_BASE_PTR) & ~(UART_BDH_SBR(0x1F)); temp3 = UART_BDH_REG(UART3_BASE_PTR) & ~(UART_BDH_SBR(0x1F));  UART_BDH_REG(UART0_BASE_PTR) = temp0 |  UART_BDH_SBR(((ubd0 & 0x1F00) >> 8)); UART_BDH_REG(UART1_BASE_PTR) = temp1 |  UART_BDH_SBR(((ubd1 & 0x1F00) >> 8)); UART_BDH_REG(UART3_BASE_PTR) = temp3 |  UART_BDH_SBR(((ubd3 & 0x1F00) >> 8)); UART_BDL_REG(UART0_BASE_PTR) = (uint_8)(ubd0 & UART_BDL_SBR_MASK); UART_BDL_REG(UART1_BASE_PTR) = (uint_8)(ubd1 & UART_BDL_SBR_MASK); UART_BDL_REG(UART3_BASE_PTR) = (uint_8)(ubd3 & UART_BDL_SBR_MASK);  /* Determine if a fractional divider is needed to get closer to the baud rate */ //brfa = (((sysclk*32000)/(baud0 * 16)) - (ubd * 32));  /* Save off the current value of the UARTx_C4 register except for the BRFA */ //temp0 = UART_C4_REG(UART0_BASE_PTR) & ~(UART_C4_BRFA(0x1F)); //temp1 = UART_C4_REG(UART1_BASE_PTR) & ~(UART_C4_BRFA(0x1F));  //UART_C4_REG(UART0_BASE_PTR) = temp0 |  UART_C4_BRFA(brfa); //UART_C4_REG(UART0_BASE_PTR) = temp1 |  UART_C4_BRFA(brfa);  Isr_InitIsr(INT_UART0_RX_TX, Uart_RxTx0_Isr); Isr_InitIsr(INT_UART1_RX_TX, Uart_RxTx1_Isr); Isr_InitIsr(INT_UART3_RX_TX, Uart_RxTx3_Isr);  // configure ISR  - UART 0 IRQ - 45 NVICICPR1 |= (1<<13); //45 MOD 32 NVICISER1 |= (1<<13); NVICIP45 = 0x30;  // priority 3. out of 15  // configure ISR  - UART 1 IRQ - 47 NVICICPR1 |= (1<<15); //47 MOD 32 NVICISER1 |= (1<<15); NVICIP47 = 0x30;  // priority 3. out of 15  // configure ISR  - UART 3 IRQ - 51 NVICICPR1 |= (1<<19); //51 MOD 32 NVICISER1 |= (1<<19); NVICIP51 = 0x30;  // priority 3. out of 15   // clear ISR flags  temp0 = UART_S1_REG(UART0_BASE_PTR); temp1 = UART_S1_REG(UART1_BASE_PTR); temp3 = UART_S1_REG(UART3_BASE_PTR); /* Enable receiver */ UART_C2_REG(UART0_BASE_PTR) |= ( UART_C2_RE_MASK | UART_C2_TE_MASK |   UART_C2_RIE_MASK | UART_C2_TIE_MASK); UART_C2_REG(UART1_BASE_PTR) |= ( UART_C2_RE_MASK | UART_C2_TE_MASK |   UART_C2_RIE_MASK | UART_C2_TIE_MASK); UART_C2_REG(UART3_BASE_PTR) |= ( UART_C2_RE_MASK | UART_C2_TE_MASK |    UART_C2_RIE_MASK | UART_C2_TIE_MASK);  }
void Isr_InitIsr(_mqx_uint isr, void (_CODE_PTR_ isr_func)(pointer)){ MY_ISR_STRUCT_PTR  isr_ptr;  isr_ptr = _mem_alloc_zero((_mem_size)sizeof(MY_ISR_STRUCT));  isr_ptr->TICK_COUNT   = 0; isr_ptr->OLD_ISR_DATA = _int_get_isr_data(isr); isr_ptr->OLD_ISR      = _int_get_isr(isr);  _int_install_isr(isr, isr_func, isr_ptr);}

 

void Uart_RxTx0_Isr(pointer user_isr_ptr){ MY_ISR_STRUCT_PTR  isr_ptr; uint_16 temp; isr_ptr = (MY_ISR_STRUCT_PTR)user_isr_ptr; isr_ptr->TICK_COUNT++;  // receive routine temp = UART_S1_REG(UART0_BASE_PTR); if (temp & UART_S1_RDRF_MASK) {  if (m_rx0Len < UART_BUF)   rx0Buf[m_rx0Len++] = UART_D_REG(UART0_BASE_PTR); } // transmit routine else if (temp & UART_S1_TDRE_MASK) {  if ((m_tx0Sent < m_tx0Len) && (m_tx0Sent < UART_BUF))  {   UART_D_REG(UART0_BASE_PTR) = tx0Buf[m_tx0Sent++];  }  else  {   // stop transmission   UART_C2_REG(UART0_BASE_PTR) &= ~(UART_C2_TIE_MASK);  } }}

 

 

View solution in original post

0 Kudos
Reply
3 Replies
2,316 Views
MichaelDavid
Contributor III

here is the solution:

void Uart_InitUart(void){ uint_32 ubd0,ubd1,ubd3,temp0,temp1,temp3,brfa; uint_32 sysclk = BSP_SYSTEM_CLOCK,busclk = BSP_BUS_CLOCK,  baud0 = 115200, baud13 = 57600; //UART configuration SIM_SCGC4 |= (SIM_SCGC4_UART0_MASK | SIM_SCGC4_UART1_MASK | SIM_SCGC4_UART3_MASK);  PORTA_PCR14 = PORT_PCR_MUX(3);      //TX 0  PORTA_PCR15 = PORT_PCR_MUX(3);      //RX 0  PORTC_PCR4  = PORT_PCR_MUX(3);      //TX 1  PORTC_PCR3  = PORT_PCR_MUX(3);      //RX 1  PORTB_PCR11 = PORT_PCR_MUX(3);      //TX 3  PORTB_PCR10 = PORT_PCR_MUX(3);      //RX 3  UART_C2_REG(UART0_BASE_PTR) &= ~(UART_C2_TE_MASK | UART_C2_RE_MASK); UART_C2_REG(UART1_BASE_PTR) &= ~(UART_C2_TE_MASK | UART_C2_RE_MASK); UART_C2_REG(UART3_BASE_PTR) &= ~(UART_C2_TE_MASK | UART_C2_RE_MASK); /* Configure the UART for 8-bit mode, no parity */ /* We need all default settings, so entire register is cleared */ UART_C1_REG(UART0_BASE_PTR) = 0; UART_C1_REG(UART1_BASE_PTR) = 0; UART_C1_REG(UART3_BASE_PTR) = 0; /* Calculate baud settings */ //ubd = (uint_32)((sysclk*1000)/(baud0 * 16)); ubd0 = (sysclk + 8 * baud0)/(16 * baud0); ubd1 = (sysclk + 8 * baud13)/(16 * baud13); ubd3 = (busclk + 8 * baud13)/(16 * baud13);   /* Save off the current value of the UARTx_BDH except for the SBR */ temp0 = UART_BDH_REG(UART0_BASE_PTR) & ~(UART_BDH_SBR(0x1F)); temp1 = UART_BDH_REG(UART1_BASE_PTR) & ~(UART_BDH_SBR(0x1F)); temp3 = UART_BDH_REG(UART3_BASE_PTR) & ~(UART_BDH_SBR(0x1F));  UART_BDH_REG(UART0_BASE_PTR) = temp0 |  UART_BDH_SBR(((ubd0 & 0x1F00) >> 8)); UART_BDH_REG(UART1_BASE_PTR) = temp1 |  UART_BDH_SBR(((ubd1 & 0x1F00) >> 8)); UART_BDH_REG(UART3_BASE_PTR) = temp3 |  UART_BDH_SBR(((ubd3 & 0x1F00) >> 8)); UART_BDL_REG(UART0_BASE_PTR) = (uint_8)(ubd0 & UART_BDL_SBR_MASK); UART_BDL_REG(UART1_BASE_PTR) = (uint_8)(ubd1 & UART_BDL_SBR_MASK); UART_BDL_REG(UART3_BASE_PTR) = (uint_8)(ubd3 & UART_BDL_SBR_MASK);  /* Determine if a fractional divider is needed to get closer to the baud rate */ //brfa = (((sysclk*32000)/(baud0 * 16)) - (ubd * 32));  /* Save off the current value of the UARTx_C4 register except for the BRFA */ //temp0 = UART_C4_REG(UART0_BASE_PTR) & ~(UART_C4_BRFA(0x1F)); //temp1 = UART_C4_REG(UART1_BASE_PTR) & ~(UART_C4_BRFA(0x1F));  //UART_C4_REG(UART0_BASE_PTR) = temp0 |  UART_C4_BRFA(brfa); //UART_C4_REG(UART0_BASE_PTR) = temp1 |  UART_C4_BRFA(brfa);  Isr_InitIsr(INT_UART0_RX_TX, Uart_RxTx0_Isr); Isr_InitIsr(INT_UART1_RX_TX, Uart_RxTx1_Isr); Isr_InitIsr(INT_UART3_RX_TX, Uart_RxTx3_Isr);  // configure ISR  - UART 0 IRQ - 45 NVICICPR1 |= (1<<13); //45 MOD 32 NVICISER1 |= (1<<13); NVICIP45 = 0x30;  // priority 3. out of 15  // configure ISR  - UART 1 IRQ - 47 NVICICPR1 |= (1<<15); //47 MOD 32 NVICISER1 |= (1<<15); NVICIP47 = 0x30;  // priority 3. out of 15  // configure ISR  - UART 3 IRQ - 51 NVICICPR1 |= (1<<19); //51 MOD 32 NVICISER1 |= (1<<19); NVICIP51 = 0x30;  // priority 3. out of 15   // clear ISR flags  temp0 = UART_S1_REG(UART0_BASE_PTR); temp1 = UART_S1_REG(UART1_BASE_PTR); temp3 = UART_S1_REG(UART3_BASE_PTR); /* Enable receiver */ UART_C2_REG(UART0_BASE_PTR) |= ( UART_C2_RE_MASK | UART_C2_TE_MASK |   UART_C2_RIE_MASK | UART_C2_TIE_MASK); UART_C2_REG(UART1_BASE_PTR) |= ( UART_C2_RE_MASK | UART_C2_TE_MASK |   UART_C2_RIE_MASK | UART_C2_TIE_MASK); UART_C2_REG(UART3_BASE_PTR) |= ( UART_C2_RE_MASK | UART_C2_TE_MASK |    UART_C2_RIE_MASK | UART_C2_TIE_MASK);  }
void Isr_InitIsr(_mqx_uint isr, void (_CODE_PTR_ isr_func)(pointer)){ MY_ISR_STRUCT_PTR  isr_ptr;  isr_ptr = _mem_alloc_zero((_mem_size)sizeof(MY_ISR_STRUCT));  isr_ptr->TICK_COUNT   = 0; isr_ptr->OLD_ISR_DATA = _int_get_isr_data(isr); isr_ptr->OLD_ISR      = _int_get_isr(isr);  _int_install_isr(isr, isr_func, isr_ptr);}

 

void Uart_RxTx0_Isr(pointer user_isr_ptr){ MY_ISR_STRUCT_PTR  isr_ptr; uint_16 temp; isr_ptr = (MY_ISR_STRUCT_PTR)user_isr_ptr; isr_ptr->TICK_COUNT++;  // receive routine temp = UART_S1_REG(UART0_BASE_PTR); if (temp & UART_S1_RDRF_MASK) {  if (m_rx0Len < UART_BUF)   rx0Buf[m_rx0Len++] = UART_D_REG(UART0_BASE_PTR); } // transmit routine else if (temp & UART_S1_TDRE_MASK) {  if ((m_tx0Sent < m_tx0Len) && (m_tx0Sent < UART_BUF))  {   UART_D_REG(UART0_BASE_PTR) = tx0Buf[m_tx0Sent++];  }  else  {   // stop transmission   UART_C2_REG(UART0_BASE_PTR) &= ~(UART_C2_TIE_MASK);  } }}

 

 

0 Kudos
Reply
2,315 Views
crezyoz
Contributor IV

HI

 

I noticed in the isr you wrote above you are using a uint16 temp var to read the S1 register. Does this have any effect since the UART regs are all 8 bit?

 

thanks~

0 Kudos
Reply
2,315 Views
MichaelDavid
Contributor III

When Initializing I wrote :

 NVICIP45 = 0x30;        // priority 3. out of 15

this turn to be interfering with the MQX kernal , changing it to 10 , (0xA0) solved the issue.

0 Kudos
Reply