clock amplitude inquiry on 32kHz crystal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

clock amplitude inquiry on 32kHz crystal

1,206 Views
darwin_deramos
Contributor I

I'm using Kinetis K81 family mcu.

In the specification for the 32kHz clock for EXTAL32 , it was specified that the typical peak-to-peak amplitude of oscillation is 0.6V and no tolerance was given.

My actual measurement on the amplitude is 0.55V.   I would like to ask if this will normally work or what voltage range should be I'm looking at.

0 Kudos
Reply
1 Reply

1,107 Views
miduo
NXP Employee
NXP Employee

Hi,

From the data sheet, there has a specification on the 32kHz OSC:

pastedImage_1.png

0 Kudos
Reply