can't work TWR-K20D72M low power mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

can't work TWR-K20D72M low power mode

1,032件の閲覧回数
bhavinmaru
Contributor III

Hello,

I am working with TWR-K20D72M EVM board as controller and i am working on Low Power Mode.

from the below link i download the TWR-K20D72M's sample codes

 

http://cache.nxp.com/files/32bit/software/KINETIS_72MHz_SRC.zip?fpsp=1&WT_TYPE=Lab%20and%20Test%20So...

 

in those sample codes there is also low power mode's sample code that code i have used.

different low power modes are given below :

 

wait : wait,VLPW

stop : stop,VLPS,LLS

power down : VLLS1,VLLS2,VLLS3

 

to test all the above low power mode sample code is given in the code which i have downloaded from the

above link.

in that code board's SW1 switch is used as wakeup source but i want to use LPTMR interrupt as wakeup source.

below i attached all my code's files.i also configured LLWU unit to wakeup using LPTMR after 9 seconds.

i used board's blue LED which will turn on when controller is wakeup after going in LLS mode(because in my

application i want that controller will go in LLS mode).this code works and controller go in LLS

mode and after 9 seconds controller is wakeup and also board's blue LED is ON.please try to solve my below

query:

 

-- controller is wakeup using LPTMR timer & also blue LED is turn ON but on terminal window it continuously

  display " ****default_isr entered on vector 3***** " i found that vector 3 is Hard Fault.

 

please give me any suggestion so that i can solve this fault or give me any other sample code for low power mode.

 

Thank You

Bhavin

Original Attachment has been moved to: low_power.zip

ラベル(1)
0 件の賞賛
返信
1 返信

919件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Bhavin,

You can download a sample package code through the link as below.

in the package code, there's a low power demo which use the corresponding pin and LPTMR to wake the MCU from the LLS mode, and please refer to it for detail.

Sample package code:

cache.nxp.com/files/32bit/software/KL25_SC.exe

Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信