audio sample code available?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

audio sample code available?

ソリューションへジャンプ
3,293件の閲覧回数
bowerymarc
Contributor V

I was reading the audio slide show presentation "Introduction to MCU Audio and USB Audio Streaming"  (http://2012ftf.ccidnet.com/pdf/0110.pdf) and I'm wondering if the code for the SoundBar Surround Processor (p.60), Headphone Audio Processor (p.61) and/or Kinetis K40 Tower SRS WOW HD SoundBar Decoder are available somewhere?

thanks,

Marc

ラベル(1)
0 件の賞賛
返信
1 解決策
2,723件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi Marc,

Sorry for the delay. The SoudBar project was the the first Audio example created for Kinetis.

Unfortunately, the Audio module was changed in new silicon revisions and this code won´t work for new devices.

Attached you can find a example of USB Speakers 96Khz 24-bits . Right now only works in Linux and Mac OS Lepoard .

I hope this helps,

Alejandro

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,724件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi Marc,

Sorry for the delay. The SoudBar project was the the first Audio example created for Kinetis.

Unfortunately, the Audio module was changed in new silicon revisions and this code won´t work for new devices.

Attached you can find a example of USB Speakers 96Khz 24-bits . Right now only works in Linux and Mac OS Lepoard .

I hope this helps,

Alejandro

0 件の賞賛
返信