Withoout S32K MCAL package

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Withoout S32K MCAL package

2,828 Views
842203661
Contributor II

Hi, 

      I have a  S32K MCAL project base on S32K14X_MCAL4_2_RTM_1_0_1. when I import and open the project in EB  tresos, EB push error:
    Plug-in with a module "Can_TS_T40D2M10I1R0" is not installed - cannot create module configurations for project "S32K146_4.2_RTM1.0.1"

    Unfortunately, the installation package  cannot be found on the NXP official website. How do I get it?

0 Kudos
Reply
4 Replies

2,818 Views
namnguyenviet
NXP Employee
NXP Employee

Hello,

Please open your EB tresos, choose Help - EB Tresos Detail. In Bundle Registry tab, check whether the Can package was installed successfully and the path of it.

 

nxf48630_0-1600072522338.png

Regards,

Nam

0 Kudos
Reply

2,813 Views
842203661
Contributor II

Without packages in the window. Because I don't have  “S32K14X_MCAL4_2_RTM_1_0_1.exe”  installation package.

I already have installation packages for V1.0.0 and V1.0.4, but are lack of V1.0.1, and this is exactly what I want.

0 Kudos
Reply

2,804 Views
namnguyenviet
NXP Employee
NXP Employee

Hello,

Your request has been processed. Please check in your Software Licensing and Support, AUTOSAR MCAL product and find in the Previous tab.

Nam

0 Kudos
Reply

2,802 Views
842203661
Contributor II

Wow! Nam, thank you very much! I get it.