Which port have internall pullup or down on MK60FN1M0VLQ12 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which port have internall pullup or down on MK60FN1M0VLQ12 ?

1,404 Views
fabriceeichenbe
Contributor I

hello,

I can't find which port have internall pullup or down on MK60FN1M0VLQ12.

I read the chapter signal multiplexing and signal description of K60 Sub-Family Reference Manual Rev. 3, November 2014 but it doesn't seem to be here.

Does anyone know where this information is ?

Yours faithfully

Fabrice Eichenberger

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,343 Views
egoodii
Senior Contributor III

I have always considered the 'lack of information to the contrary' to indicate that ALL GPIO pins have full port-control-options, including pull-enable and pull-direction.  This is in contrast, for instance, with the K22P121M100SF9RM.pdf table 10-2, that lists 'GPIO limitations' for that part, although even in THAT case pull-enable and pull-direction are available on all ports/pins.

1,343 Views
fabriceeichenbe
Contributor I

OK, thank you :smileyhappy:

0 Kudos
Reply