Where is K40Z memory map for peripherals?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where is K40Z memory map for peripherals?

1,484 Views
LouisVRuffino
Contributor I


The datasheet refers to a Bit Manipulation Engine and the Analog section refers to a 12 bit ADC mode and a <12 bit mode.

Where are the programmers reference manual to these peripherals? where is the peripheral memory map for the device?

0 Kudos
Reply
2 Replies

1,412 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Louis,

Actually, The K40 hasn't the BME (Bit Manipulation Engine) module after I checked the reference manual.

So I was wondering if you can upload the datasheet.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,412 Views
qqenchoi
Contributor I

sdcscfsdfvsaxdcaxvfdgvbdfgvedf

0 Kudos
Reply