Where is Flex Bus on the MK22FX1M0VLL12

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where is Flex Bus on the MK22FX1M0VLL12

2,883件の閲覧回数
brentgreenwald
Contributor III

In the datasheet for the MK22FX1M0VLL12 the flexbus AD pins 21-23 are missing. Is there any reason why they are not included on the master pin out list? Or is there some other approach to wiring the 32 bit flex bus.

ラベル(1)
タグ(2)
0 件の賞賛
返信
3 返答(返信)

2,702件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

For the pin resource limitation, the PTB[6~8] were removed from MK22FN1M0VLL12 , which is pin ALT5 function is FB_AD[21:23].

There could not do 32 bit data operation via MK22FN1M0VLL12 Flexbus module.

Customer could select K22 product such as MK22FN1M0VLQ12 or MK22FN1M0VMC12R as a replacement(if customer need to connect external 32-bit port size memory).


Thank you for the attention.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,702件の閲覧回数
brentgreenwald
Contributor III

But then why dose the chip say it supports 32 bit?

0 件の賞賛
返信

2,702件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Thank you for the info. The MK22FN1M0VLL12 reference manual should be updated about related Flexbus module.

I will forward related info to Kinetis product team about this document issue.

Sorry for that may bring any inconvenience to you.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信