What's the programmer to use in Family KL02?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What's the programmer to use in Family KL02?

1,777 Views
hnicolasg
Contributor I

I'm going to begin with MCU freescale and the KL02 is appropriate to my project.

What's the best Freedom Development Platform for Kinetis?

0 Kudos
Reply
3 Replies

1,626 Views
mjbcswitzerland
Specialist V

Hi Hector

For the KL02 the FRDM-KL02Z is the obvious choice - Freescale Freedom Development Platform for th|Freescale

Regards

Mark

Kinetis: µTasker Kinetis support

KL02: µTasker FRDM-KL02Z support

For the complete "out-of-the-box" Kinetis experience and faster time to market

1,626 Views
hnicolasg
Contributor I

Thank you !!..

Yes, but i believed that there was one generic..

Thank you so much.

Now, I need buy one.

.

0 Kudos
Reply

1,626 Views
dave408
Senior Contributor II

What's nice is that the freedom boards are so inexpensive!  Under $13 for the lower-powered Kinetis processors.  I'm not sure which, if any of the Segger firmwares will give you debugging capability in KDS, though (SEGGER - The Embedded Experts - OpenSDA / OpenSDA V2

0 Kudos
Reply