What's the difference between 'USB serial port' and 'USB-UART'?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What's the difference between 'USB serial port' and 'USB-UART'?

ソリューションへジャンプ
3,740件の閲覧回数
jelean
Contributor I

I find a USB serial port and a USB-UART at the same time on my PC,but I don't know the difference between them.Who can tell me? A lot of thanks! By the way I can't find the driver for the USB-UART(I was testing a USB demo of FRDM-KL25Z) and where can I download the dirver?


2.png

ラベル(2)
0 件の賞賛
返信
1 解決策
2,306件の閲覧回数
JimDon
Senior Contributor III

You have two usb cords plugged in - one the the usb-serial converter that is on the OpenSDA, the other is the code you are running on the board. Pleas read the docs that came with the board.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,307件の閲覧回数
JimDon
Senior Contributor III

You have two usb cords plugged in - one the the usb-serial converter that is on the OpenSDA, the other is the code you are running on the board. Pleas read the docs that came with the board.

0 件の賞賛
返信
2,306件の閲覧回数
jelean
Contributor I

Got it! Thank U!

0 件の賞賛
返信