What is the operating temperature range for the TRK-KEA128?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the operating temperature range for the TRK-KEA128?

1,016 Views
chadcarius
Contributor I

As above, for the populated board, what it is operating temperature range?

0 Kudos
Reply
1 Reply

933 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Chad Carius,

   We just have the KEA128 chip temperature range:  -40 to 125°C.

  Normally, the PCB board can endure about 150°C . But  because different electric component have different operating temperature range, you also need to check the other components on the board.

  

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply