What is the Appropriate Configuration for K65 @120 MHz Operation using 32K External Oscillator

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the Appropriate Configuration for K65 @120 MHz Operation using 32K External Oscillator

1,299 Views
johngreene
Contributor I

What is the appropriate configuration to run the K65 at 120MHz without an external 16MHz oscillator?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,157 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi  john,

You can't configure K65 @120 MHz using 32K External Oscillator.

When using 32K external oscillator, the FLL is needed.

Calculation 120MHz = 2929 × fFLL_ref ,  then the fFLL_ref need to be equal to 40969.6Hz.

Best Regards,

Robin

0 Kudos
Reply