What is the Appropriate Configuration for K65 @120 MHz Operation using 32K External Oscillator

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What is the Appropriate Configuration for K65 @120 MHz Operation using 32K External Oscillator

1,264 次查看
johngreene
Contributor I

What is the appropriate configuration to run the K65 at 120MHz without an external 16MHz oscillator?

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

1,122 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi  john,

You can't configure K65 @120 MHz using 32K External Oscillator.

When using 32K external oscillator, the FLL is needed.

Calculation 120MHz = 2929 × fFLL_ref ,  then the fFLL_ref need to be equal to 40969.6Hz.

Best Regards,

Robin

0 项奖励
回复