USB bootloader on Kinetis?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB bootloader on Kinetis?

2,753 Views
OldNick
Contributor IV

There used to be an appnote AN3927 describing a simple USB flash application, has this been ported to Kinetis, and made to work with MQX?

 

Thanks

0 Kudos
Reply
1 Reply

2,187 Views
mjbcswitzerland
Specialist V

Hi

 

The following USB boot loader is available for the Kinetis (K60 and K40)

http://www.youtube.com/watch?v=H4TYM9jY2-g

 

It is however not MQX based...but is has been used to load MQX applications (just the link address needs to be changed to match).

 

Regards

 

Mark

 

0 Kudos
Reply