USB Port of K60

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Port of K60

1,086 Views
leofavilli
Contributor I

Hi All,

I'm developing a new project based on K60 device and I would like implement two USB interface. One in FS mode, using internal FS PHY and one in HS mode using external PHY. Could they work together or there are some restriction.

 

After that HS mode port could work in HOST configuration with DMA forward internal RAM of K60, just to satisfy a input data rate of 50Mbit/s.

 

Thank you

0 Kudos
Reply
0 Replies