USB Audio speaker

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Audio speaker

1,770 Views
kyleyang
Contributor IV

Hi

I used FRDM-K66F to created a USB audio speaker application based on K21F KSDK 2.0 USB example code.

Basically the function is works in 16bit/16kHz, but when I try to increase the sample rate to 48kHz.

The function is not works.

Is there any one have similar experience before?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,577 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Customer also could refer KSDK software for TWR-K65F180M board [usb dev_audio_speaker] demo.

For the FRDM-K66F use the different codec chip DA7212, customer need to check the DA7212 codec driver related codes. 


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply