UART and pin mux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART and pin mux

1,915件の閲覧回数
Keith4DSmith
Contributor V

A UART consists of four pins TX, RX, CTS_b, and RTS_b.

Is it required that all pins of a UART be on the same port, or can any combination of pins be used?

ラベル(1)
タグ(2)
1 返信

1,733件の閲覧回数
mjbcswitzerland
Specialist V

Keith

You can use any pins belonging to a UART. Eg. UART1_TX on PTB5 or PTE11, UART1_RX on PTB6, PTE12 or PTA17, UART1_RTS on PTB7 or PTE13 and UART1_CTS on PTB14 or PTA22 or PTD2 (ports examples illustrative and probably done match a physical device).

What you can't do is use UART1_CTS and UART1_RTS with UART2_TX and UART2_RX (at least not in one of the automated modem modes).

Not all RTS and CTS pins are necessarily available (some UARTs or LPUARTs done have or support them) and RTS/CTS operation (RTS/CTS flow control and RS485 control) can usually be emulated with GPIOs in such cases if absolutely necessary.

Regards

Mark