Two induvidual I2S Streams on K20 72mhz

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Two induvidual I2S Streams on K20 72mhz

1,660件の閲覧回数
tobias_strate
Contributor I

Hello 
i have moderate amount of Experience with Kinetis Studio and processor expert. 
I am working on a project which contains an I2S to S/PDIF Codec and an audio codec. I will need to send an receive to both of these simultaneously. 

From the datasheet of the K20 processor i see that it should be able to handle two I2S streams yet i cannot find how to set it up, i know the DMA needs to move the data back and forth but which registers do i move the data from and to? 

I think i am quite lost on this one, hope someone can throw me a rope. 

Best Regards 

Tobias T. Strate 

0 件の賞賛
返信
3 返答(返信)

1,571件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi Tobias,

If you want to call a DMA transfer when  I2S received data, the I2S Rx is the DMA source. Conversely, if you want to call a DMA transfer when I2S need more data, the I2S Tx is the DMA source.There is a DMA request source table in K20P100M72SF1RM.pdf page 80. You can set corresponding number to DMAMUX's register.

There are some resource you can refer to. If you have download K20 SDK package, please refer to SDK_2.2_MK20DN512xxx10\boards\twrk60d100m\driver_examples\sai\edma_transfer.

Although it works in SAI mode, the dma setting is useful.

You can also refer to AN4800 which you can find on NXP website.

Hope my suggesting will be useful to you

Regards

0 件の賞賛
返信

1,571件の閲覧回数
tobias_strate
Contributor I

i have tried making a setup purely with the Init components, but it is not working, it seems to be the DMA and I2S interrupt which is not working. i have added the PE_ISR(DMA_interrupt) to Events.C. Yet it never seems to be called, 

0 件の賞賛
返信

1,571件の閲覧回数
tobias_strate
Contributor I

Thanks alot. 
i will take a look at it. 

0 件の賞賛
返信