Trouble resetting Periodic Interrupt Timer (PIT)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Trouble resetting Periodic Interrupt Timer (PIT)

2,635 Views
ignisuti
Contributor IV

I’m trying to synchronize this timer module with another time source.

According to the documentation, I can restart this timer by simply disabling and re-enabling it. I've set a break point immediately before and after the code listed below. I don’t think this is working as intended because the timer’s Current Value is decremented slightly and nowhere near the Reload Value.

PIT_TCTRL_REG( PIT_BASE_PTR, 0 ) &= ~PIT_TCTRL_TEN_SHIFT;

PIT_TCTRL_REG( PIT_BASE_PTR, 0 ) |=  PIT_TCTRL_TEN_SHIFT;

Note: I’m referencing Figure 38-23 of the Document K10P144M100SF2RM Rev. 6, Nov 2011

Please let me know if you have any suggestions.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,871 Views
mjbcswitzerland
Specialist V

Hi

I think that you may need to write to the LDVAL register when the PIT is disabled so that it restarts.

This is an extract from the PIT code from the uTasker project which can be used as a single-shot / retriggerable or periodic timer - it was necessary to disable operation if its value was to be reset/retriggered - without this it doesn't react.

if (PIT_settings->mode & (PIT_SINGLE_SHOT | PIT_RETRIGGER)) {  // single shot always behaves as retriggerable - periodic change at next timeout by default but can be forced with PIT_RETRIGGER                

    ptrCtl->PIT_TCTRL = 0;    // disable PIT so that it can be retriggered if needed

}

ptrCtl->PIT_LDVAL = PIT_settings->count_delay;               // load interval value

ptrCtl->PIT_TFLG  = PIT_TFLG_TIF;                            // clear pending interrupts

ptrCtl->PIT_TCTRL = ulCommand;                               // start PIT with interrupt enabled, when handler defined

Regards

Mark

http://www.uTasker.com