TWR-KV58F220M application cannot enter into interrupt

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TWR-KV58F220M application cannot enter into interrupt

2,967 次查看
Roger_WANG_2022
Contributor I

boot: flash-resident bootloader

peripherals: uart

IDE: MCUXpresso IDE

SDK Version: SDK_2_8_0_TWR-KV58F220M.zip

boot example: twrkv58f220m_tower_bootloader

Application example:twrkv58f220m_led_demo_tower_a000

Tool: KinetisFlashTool.exe

after update, four led blinks one by one, everything was all right. But when i add some other resource (for example SPI), application was stop in the DefaultISR. What's the reason? why application cannot enter into the right ISR?

Kind regards,

Roger

标签 (1)
0 项奖励
回复
3 回复数

2,934 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Roger,

There are several SPI examples in SDK_2_8_0_TWR-KV58F220M. Do you have reference to its peripheral initialization code and interrupt settings?

twrkv58f220m_dspi_interrupt.png

You can upload a simple test project so that I can quickly analyze the cause of the problem.

Best Regards,
Robin

0 项奖励
回复

2,896 次查看
Roger_WANG_2022
Contributor I

Hi,Robin

I think i have find the bug. It's the startup file problem.

the example twrkv58f220m_led_demo_tower_a000 use "startup_MKV58F24.S".

and normal example use "startup_mkv58f24.c".

the SDK support two different example based on "KSDK driver" or "transactional API".

the difference is "KSDK driver" use SPI0_IRQHandler directly, "transactional API" use SPI0_DriverIRQHandler which not define in "startup_MKV58F24.S".

I hope NXP engineer can fix this bug. I waste nearly one week time on this problem, hope these can help other NXP users. Thank you!

Best Regards,
Roger

0 项奖励
回复

2,924 次查看
Roger_WANG_2022
Contributor I

Hi, Robin

Thanks for your reply. I use "dspi_interrupt_b2b_transfer_master" from SPI examples in SDK_2_8_0_TWR-KV58F220M. And the test projects are attached.

I also search some relate topic,

https://community.nxp.com/t5/S32K/s32k148-bootloader-to-app-can-t-work-interrupt/m-p/1165845

unfortunately don't get the right answer.

Best Regards,

Roger

0 项奖励
回复