TWR-K60N512 and eGUI HelloWorld

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-K60N512 and eGUI HelloWorld

6,416 Views
Glogov_Kolac
Contributor II

Does anybody have succes with eGUI 2.01 HelloWorld example running under MQX 3.7 RTOS. 

I try this example but there is no text, image or any kind of content on TWR LCD. To mention that I am using elevatro SPI rather than 16b mode. Is there anyone who have succes with this example and how ?!

0 Kudos
Reply
10 Replies

5,760 Views
Gargy
NXP Employee
NXP Employee

Hi,

 on latest release of eGUI on web is example with K60 and eGUI over SPI.

 

Good luck

 

0 Kudos
Reply

5,760 Views
Glogov_Kolac
Contributor II

I have tryed all examples for TWR K60N512 in eGui 2.01 (baremetal, mqx 3.7 and 3.6) and after running the code there is no content on my TWR LCD. I configured it to use external SPI (SW1 = 01111110). If somebody have succes with this example and how ?

0 Kudos
Reply

5,760 Views
Gargy
NXP Employee
NXP Employee

The examples, should work correctly.

The issue could be done by HW, did you tried the LCD on any other MCU? TWR-MCF51CN128 ??

 

 

0 Kudos
Reply

5,760 Views
Glogov_Kolac
Contributor II

TWR LCF works fine with builtin demo (driven by onboard Coldfire JM128 MCU). The problem is when I try to run demo from my Kinetis TWR Mcu acros the elevator board bypasing JM128. Is there some extra config on HW or SW for External SPI running ?

0 Kudos
Reply

5,760 Views
Dekiru
Contributor IV
Hi, - Did you clear the JM128 chip? If not, there should be conflict and you may not be able to use LCD - I think that there is conflict between LCD interface and Flexbus, so try to not use flexbus (and MRAM of course) when using TWR LCD Regards
0 Kudos
Reply

5,760 Views
Gargy
NXP Employee
NXP Employee

Good point, I forgot on this .

 

I§m ussually using this simple project (CW 6.3).

0 Kudos
Reply

5,760 Views
Glogov_Kolac
Contributor II

I will try to solder pins of reset taster in order to keep JM128 in reset all the time. This is (IMHO) better idea than flashing JM (besides that I dont have BDM flasher). 

0 Kudos
Reply

5,760 Views
Gargy
NXP Employee
NXP Employee

Hi,

 on TWR-LCD JM128 is some kind of bootloader that you could use instead of BDM. :smileyhappy:

 

 

0 Kudos
Reply

5,760 Views
LuisCasado
NXP Employee
NXP Employee
Hello Here you can find a valid app for working with eGUI and JM will not cause interferences. Notice that not only the reset line is the issue but touch screen control. http://www.towergeeks.org/forum/topics/twrk60n512-and-tft best regards Luis
0 Kudos
Reply

5,760 Views
LuisCasado
NXP Employee
NXP Employee
I forgot tell you that you can use bootloader for flashing Luis
0 Kudos
Reply