TWR-K60F120M doesn't work with TWR-SER2.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-K60F120M doesn't work with TWR-SER2.

1,236 Views
rogerdoak
Contributor I

I am able to use the TWR-K60F120M with the TWR-SER, run the hid example, and get the mouse and keyboard to work just fine.  However I need to run high speed USB with the TWR-SER2.  I shunted J21 as instructed for high speed USB but it does not work.  I can't even run the application.  I tried changing BSP_USB_TWR_SER2 to 1 in twrk60f120m.h but that didn't help.  Thanks for your help.

Labels (1)
0 Kudos
Reply
1 Reply

1,009 Views
hectorsanchez
Contributor IV

If you are using MQX try this:

  

enable HS driver

  

#define USBCFG_DEFAULT_DEVICE_CONTROLLER (&_bsp_usb_dev_ehci0_if)

#define USBCFG_DEFAULT_HOST_CONTROLLER (&_bsp_usb_host_ehci0_if)

  

And rebuild libraries.

This works on the TWR-K70 , try it on the TWR-K60

Also, In the USB stack, you need to setup HIGH_SPEED_DEVICE to 1 in user_config.h in each USB stack project you want to test with TWR-SER2.

0 Kudos
Reply