TWR-K60F120M and TWR-LCD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TWR-K60F120M and TWR-LCD

1,342件の閲覧回数
michael_wahler
Contributor III

Hi,

I just bought a TWR-LCD module for my TWR-K60F120M kit. Where can I find a hello world application for using the lcd screen with the K60? I'd like to print some text and draw some lines.

Also, I don't quite understand the TWR-LCD manual. What is the correct jumper configuration for controlling TWR-LCD from the K60?

Kind regards

Michael

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 返信

1,145件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

TWR-LCD module settings:

     - touch screen through elevator: SW5 must have sets all switches to ON.

     - LCD SPI through elevator: switch are set up with in follow sequence "01111110".

     - LCD flexbus 16 bits through elevator: switch are set up with in follow sequence "10111110".

     - LCD SPI with onboard MCF51JM128: switch are set up with in follow sequence "01001110".

Regards,

Luis

0 件の賞賛
返信