TWR-K60F120M and TWR-LCD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-K60F120M and TWR-LCD

1,357 Views
michael_wahler
Contributor III

Hi,

I just bought a TWR-LCD module for my TWR-K60F120M kit. Where can I find a hello world application for using the lcd screen with the K60? I'd like to print some text and draw some lines.

Also, I don't quite understand the TWR-LCD manual. What is the correct jumper configuration for controlling TWR-LCD from the K60?

Kind regards

Michael

Labels (1)
0 Kudos
Reply
1 Reply

1,160 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

TWR-LCD module settings:

     - touch screen through elevator: SW5 must have sets all switches to ON.

     - LCD SPI through elevator: switch are set up with in follow sequence "01111110".

     - LCD flexbus 16 bits through elevator: switch are set up with in follow sequence "10111110".

     - LCD SPI with onboard MCF51JM128: switch are set up with in follow sequence "01001110".

Regards,

Luis

0 Kudos
Reply