TWR-K60D100M USB problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TWR-K60D100M USB problem

1,343件の閲覧回数
MWMinor
Contributor V

Hi

Can anyone help me with a problem I have trying to get the USB port on the TWR-SER board to work as a CDC device...?

I've checked links on the TWR-SER board and they are correct;

pastedImage_0.png

and tried using both the virtual com port and the mouse example but neither work.....and by working I mean that when I plug the mini-usb connector to a spare USB port on my laptop, the laptop just doesn't see it.

I've tried another laptop - but that made no difference.

I know the port on the TWR-SER card works, as when I tried the HVAC demo, the boards respond when the USB stick is plugged in it enumerates and mounts the disk.

If anyone has any suggestions they would be really appreciated.

Ken

0 件の賞賛
返信
1 返信

1,129件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Ken:

We are sorry you did not receive help with this issue before. I see you just posted a new thread in the following link:

Problem with USB enumeration on K60 board

I will follow up with you with that new one.

Regards!
Jorge Gonzalez

0 件の賞賛
返信