TWR-K53N512 with MED-EKG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-K53N512 with MED-EKG

1,254 Views
soumyaks
Contributor II

Hi,

I was just trying to use the TWR-K53N512 with MED-EKG. But as given in UserGuide, I donot have a TWR-SER. Can I use a TWR-K70F120M instead for connectivity?  Can I also get pointers on building this tower system?

Many Thanks,

Soumya

0 Kudos
Reply
1 Reply

1,075 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Soumya  KS,

    Please give me what the userguide you are reading.

    You can't use the TWR-K70F120M board instead of TWR-SER. But you can check it, what the detail function used with TWR-SER, you can find other hardware to replace. Take an example, if it is just use the UART, you can find a TTL to USB tool to replace the TWR-SER.

    But to work easily, it's better to work with TWR-SER:

Serial (USB, Ethernet, CAN, RS232/485) Tower System Module|NXP 

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply