TWR-K21F120M link beaglebone use USB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TWR-K21F120M link beaglebone use USB

2,396件の閲覧回数
張峻瑞
Contributor I

Dear sir, I have a architecture like this

115654lhh1ifem97ejr7e7.png

I can`t find TWR-K21F120M USB Device Demo(only CDC), can you give me the USB Device Demo (Bulk mode)?

*Beaglebone USB Host is ready

Thank you very much

ラベル(1)
タグ(3)
0 件の賞賛
返信
4 返答(返信)

2,180件の閲覧回数
adriancano
NXP Employee
NXP Employee

Hi,

You can download the KSDK standalone version for the TWR-K21F120M from HERE under the tab Software Development Kits.

The KSDK includes examples for different USB classes, following the path: C:\Freescale\KSDK1.1.0_K21FA_1.0.0\usb\example\device

Please refer to the Integration of the USB Stack and Kinetis SDK document (C:\Freescale\KSDK1.1.0_K21FA_1.0.0\usb\doc) to know how to build an run the examples.


Hope this information can help you

Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,180件の閲覧回数
張峻瑞
Contributor I

I download and install KSDK1.1.0_K21FA_1.0.0, then import C:\Freescale\KSDK1.1.0_K21FA_1.0.0\usb\example\device\hid.

But has lot file not find, how can I do? 

Thanks very much.

1.jpg

0 件の賞賛
返信

2,180件の閲覧回数
adriancano
NXP Employee
NXP Employee

Hi,

The KSDK is not supported by CodeWarrior, the IDEs that support KSDK are:

  • KEIL MDK/uVision.
  • Kinetis Design Studio IDE.
  • Atollic TrueSTUDIO.
  • ARM GCC

You can find the complete information about the KDS IDE HERE.


Hope this information can help you

Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,180件の閲覧回数
mjbcswitzerland
Specialist V
0 件の賞賛
返信