TSI noise mode KL16

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TSI noise mode KL16

2,058件の閲覧回数
alexandermaurer
Contributor I

Hello,

like described in the Refmanual (KL16P80M48SF4RM) chapter 41.4.13.1  Automatic noise mode.

Who can explain the confusing Block Diagram Figure 41-17. What register were the counter bits taken from? and how is the combination of the Filter bits and DVolt control bits working together. The datasheet is confusing within this chapter.

Furthermore when using noise detection mode  chapter 41.4.13 the description is clear until number 10. What to do with the value of Rs and Dvolt in the end?

Thank you in advanced!

ラベル(2)
タグ(4)
0 件の賞賛
返信
2 返答(返信)

1,791件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi 

with Rs and Dvolt you can select the best option of DVOLT[1:0], EXTCHRG[2:1] and EXTCHRG[0] 

Please check table 43-13.

I recomend  you that you use the TSS library, instead or use only the TSI module.

regards

Vicente Gomez

0 件の賞賛
返信

1,791件の閲覧回数
alexandermaurer
Contributor I

Mr Salazar,

thank you for answering. Your answer doesnt help me a lot, because what you have written is already described in the datasheet.

0 件の賞賛
返信