System oscillator will not start

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

System oscillator will not start

ソリューションへジャンプ
4,020件の閲覧回数
aune
Contributor III

Using the FRDM-K22F ( MK22FN512VLH12 ), and trying to use the external crystall.

After setting up the HGO = 1, Range = 1 and EREFS = 1, and selecting CLKS = 2 I would assume that the oscillator should start, but nothing happens.

I have verified that R57 is not present on the PCB.

0 件の賞賛
返信
1 解決策
3,786件の閲覧回数
mjbcswitzerland
Specialist V

Hi

The gain setting must match with the HW.

If the crystal is not loaded (no loading capacitors or feedback resistor) the low gain is correct. Setting high gain will be wrong and not work.

If the crystal is loaded (with loading capacitors and a feedback resistor) the high gain is correct. Setting low gain will be wrong and not work.

Some Freescale boards require high gain and some require low gain.

If it is not clear from the circuit see which one works and use that.

Regards

Mark

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,786件の閲覧回数
aune
Contributor III

If I don't set the HGO = 1, but leave this at 0, it works. ANyone got a good explanation why?

0 件の賞賛
返信
3,786件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,

In the External Crystal/Resonator Connections section, it illustrates the various external crystal/resonator connections of the corresponded oscillator mode.

And please refer to it in details.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,786件の閲覧回数
mjbcswitzerland
Specialist V

Hi

The gain setting must match with the HW.

If the crystal is not loaded (no loading capacitors or feedback resistor) the low gain is correct. Setting high gain will be wrong and not work.

If the crystal is loaded (with loading capacitors and a feedback resistor) the high gain is correct. Setting low gain will be wrong and not work.

Some Freescale boards require high gain and some require low gain.

If it is not clear from the circuit see which one works and use that.

Regards

Mark

0 件の賞賛
返信
3,786件の閲覧回数
aune
Contributor III

Thanks for the explanation, makes sense.

As you said, I have no external feedback resistor, so when setting HGO = 0, the oscillator started up just fine.

0 件の賞賛
返信