Support for KW21Z?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Support for KW21Z?

1,271件の閲覧回数
tommarble
Contributor I

I'm considering the part MKW21Z512VHT4 for 802.15.4 6LoWPAN applications as the feature set is very impressive:

Kinetis KW21Z 2.4 GHz|ARM Cortex-M0+|32-bit MCUs|NXP

However the links on that page "NXP Sales Office" and "NXP Authorized Distributor" are broken :smileysad:

The KSDK (Introducing Kinetis SDK v2 ) doesn't list KW21Z as supported (and seems to be software only).

The competitive part I'm considering is the TI CC2538 http://www.ti.com/product/cc2538/

which has a hardware SDK: http://www.ti.com/tool/cc2538dk​

and an application reference design:  http://www.ti.com/product/CC2538/datasheet/applications_implementation_and_layout#SWRS0969738

DigiKey lists the part, but it is not available: MKW21Z512VHT4 Freescale Semiconductor - NXP | Integrated Circuits (ICs) | DigiKey

Does anyone have an idea

  • When the KW21Z will be shipping?
  • Will there be application reference designs?
  • Will there be a hardware SDK?

Thanks!

--Tom

ラベル(1)
0 件の賞賛
返信
1 返信

1,152件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

KW21Z R1.0 silicon is on pre-production status and will not shipping to ordinary customer at present. Full release will at Sep 2016. We will provide FRDM and USB Dev board accordingly.

B.R.

Fang

0 件の賞賛
返信