Size of Azure Iot Middleware

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Size of Azure Iot Middleware

1,316件の閲覧回数
pritesh_shah
Contributor I

Dear All,

I want to use Azure IoT middleware for my application with Kinetis K64 controller but having following questions.

How much flash memory is required to run azure IoT application ?

what is the size of Azure IoT stack with umqtt after build it ?

タグ(1)
0 件の賞賛
返信
1 返信

1,269件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello,

Hope you are doing well. 

I recommend to read the following post from the Azure website on the recommendation for minimum space needed.

I'd recommend to test the examples provided in the SDK. The amount of memory it covers will be listed in the .map file.

Best Regards,

Sabina

0 件の賞賛
返信