Secure application code that besides in Flash Memory for MKE18F512V.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Secure application code that besides in Flash Memory for MKE18F512V.

1,463 Views
rohitchudasama
Contributor III

I use MKE18F512V controller. I have my application code in flash memory. But how to secure that code so no one can retrieve from hardware (MKE18F512V) . I mean how to protect the flash memory to access from outside.

Thanks

0 Kudos
Reply
1 Reply

1,366 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please refer the application note: AN4507 Using the Kinetis Security and Flash Protection Features.

Wish it helps. Have a great day!

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply