Secure Device won't boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Secure Device won't boot

Jump to solution
2,548 Views
ivekengineer
Contributor III

I am trying to secure my flash memory (setting the FSEC to 0xFF) using my JTAG debugger.   I do seem to be modifying the proper location in flash memory.  When I try to re-attach my debugger after programming, it does indicate that the device is secure.

The issue is that my firmware does not seem to execute properly after securing the device.  It is either not booting up, or is hanging somewhere in the code.  Since I cannot attach my JTAG debugger, I can not easily figure out what is going on.  I do not see any such problem when the device is unsecure.

From what I understand, securing the flash memory is only supposed to inhibit external access to flash memory from the JTAG debugger - so what else could possibly be going on here?

I am using a KV58F1M0VLQ24, a PE Multilink FX, and also trying a PE Cyclone Max.  I am also programming the FOPT bit to 0xFB to inhibit NMI interrupts.

Labels (1)
Tags (1)
1 Solution
2,405 Views
ivekengineer
Contributor III

I finally figured it out.  Bits FBSL of SIM_SOPT2 determine the FlexBus security level.  The reset default is 00 which does not allow off-chip accesses (instruction and data) via the FlexBus when the flash security is enabled.  I changed this value to 10 and now off-chip data access is allowed.  My LCD and some of my LEDs are on the FlexBus, so a lack of data access made it appear that the device wasn't even booting.  Now, everything seems to be working fine.

View solution in original post

1 Reply
2,405 Views
ivekengineer
Contributor III

I finally figured it out.  Bits FBSL of SIM_SOPT2 determine the FlexBus security level.  The reset default is 00 which does not allow off-chip accesses (instruction and data) via the FlexBus when the flash security is enabled.  I changed this value to 10 and now off-chip data access is allowed.  My LCD and some of my LEDs are on the FlexBus, so a lack of data access made it appear that the device wasn't even booting.  Now, everything seems to be working fine.