Sample code I2S for MK20DX128VLH5 repost

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Sample code I2S for MK20DX128VLH5 repost

2,900件の閲覧回数
afdasdfas
Contributor II

Hi all. Does any one have sample code or project  I2S for Kinetis MK20DX128VLH5 Or code of any any kinetis MCU ? I try to find it so much, but don't see any thing to refer . I need to build I2S for audio use MK20DX128VLH5.  But There are too little information or tutorial or support or project about Kinetis.

タグ(1)
0 件の賞賛
返信
4 返答(返信)

2,156件の閲覧回数
carlos_neri
NXP Employee
NXP Employee

take a look to this thread, it has an example that might be useful:

https://community.freescale.com/message/81904#81904

0 件の賞賛
返信

2,156件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

Have you seen these AN?

http://cache.freescale.com/files/32bit/doc/app_note/AN4369.pdf?fpsp=1&WT_TYPE=Application Notes&WT_VENDOR=FREESCALE&WT_FILE_FORMAT=pdf&WT_ASSET=Documentation

http://cache.freescale.com/files/32bit/doc/app_note/AN4800.pdf?fpsp=1&WT_TYPE=Application Notes&WT_VENDOR=FREESCALE&WT_FILE_FORMAT=pdf&WT_ASSET=Documentation

Luis

2,156件の閲覧回数
afdasdfas
Contributor II

Hi

Thank you. These AN are helpful for me to know I2S, but i donot know the way to build the actual I2S project on CodeWarrior . Do you have any project about i2s which i can refer to build my project ?

Huynh Viet Phuong

0 件の賞賛
返信

2,156件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

Do you mean that you can't build the software projects associated to the application notes?

Luis

0 件の賞賛
返信