SWO TRACE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SWO TRACE

2,246 Views
LArmstrong1985
Contributor III

Good morning,

is possible to use SWO Trace with OpenSDA on Kinetis K64 board?

And if I use a second board as a SWD programmer?

What I have to do to enable it?

Thank you very much!

Labels (1)
Tags (1)
3 Replies

2,167 Views
ErichStyger
Specialist I

OpenSDA does not support SWO.

You need an external debug probe which is capable dealing with SWO, e.g. see ARM SWO Performance Counters | MCU on Eclipse 

See as well:

Tutorial: Using Single Wire Output SWO with ARM Cortex-M and Eclipse | MCU on Eclipse 

I hope this helps

Erich

2,167 Views
LArmstrong1985
Contributor III

Kinetis board as external debugger has SWO pin that I can use it to SWO Trace is right?

swo-trace-connected-to-debug-header.png

Do I also have to do something on firmware/project to allow its use?

0 Kudos
Reply

2,167 Views
ErichStyger
Specialist I

No, you cannot use an external Kinetis as debugger to take advantage of the SWO pin, as that external Kinetis boards would run OpenSDA. As pointed out below: it is not possible to use SWO with OpenSDA because the OpenSDA firmware does not support SWO. The hardware (debug connector) would support it, but not the OpenSDA.

So: you need an external debug probe capable for SWO, either a SEGGER, a P&E or a LPCLink2 probe (as shown in above article).

You don't have to do anything in your application/firmware: the probe firmware will handle everything.