SDRAM and Parallel NOR flash interfacing with MK26FN2M0VLQ18

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDRAM and Parallel NOR flash interfacing with MK26FN2M0VLQ18

1,055 Views
prasannanaik
Contributor III

Hi,

   I want to interface SDRAM and Parallel NOR flash with MK26FN2M0VLQ18. There's not much information on the flexbus interface. Can i get some documents regarding flexbus?.Also can you also suggest some application note regarding the same.

Thanks,

Prasanna

0 Kudos
Reply
1 Reply

970 Views
miduo
NXP Employee
NXP Employee

Hello,

You may would like to make reference this application note on "Multiplexing Pins Between SDRAM and
FLEXBUS on K65/K66"  https://www.nxp.com/docs/en/application-note/AN5095.pdf 

  K65 is a superset of the K26 with Ethernet.

0 Kudos
Reply