Regarding TWR-K70F120M-SCH, JTAG connection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Regarding TWR-K70F120M-SCH, JTAG connection

1,973 次查看
puspamnayak
Contributor III

Hi,

I am using MK70FN1M0VMJ12 in my project and referring TWR-K70F120M-SCH. I found in Tower board in JTAG connection TMS is pulled-up using 10k and when i looked into the reference manual (page 259), its mentioned that K70 has internal Pull-up for TMS.

So want to know why one more pull-up of 10K was used in Tower boad ?

Kindly reply ASAP

Thanks and regards,

Puspam N

标记 (2)
0 项奖励
回复
2 回复数

1,857 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Puspam U,

The debug signals are multiplexed with general purpose I/O pins, so some signals will require proper biasing to select the operating mode.

And the JTAG_TMS signal on PTA3 requires a strong pullup resistor for mode selection.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,857 次查看
puspamnayak
Contributor III

Hi Jeremyzhou,

Thanks for giving technical  clarification.

Have a nice day !

Thanks once again

Regards,

Puspam

0 项奖励
回复