Regarding TWR-K70F120M-SCH, JTAG connection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Regarding TWR-K70F120M-SCH, JTAG connection

1,974件の閲覧回数
puspamnayak
Contributor III

Hi,

I am using MK70FN1M0VMJ12 in my project and referring TWR-K70F120M-SCH. I found in Tower board in JTAG connection TMS is pulled-up using 10k and when i looked into the reference manual (page 259), its mentioned that K70 has internal Pull-up for TMS.

So want to know why one more pull-up of 10K was used in Tower boad ?

Kindly reply ASAP

Thanks and regards,

Puspam N

タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,858件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Puspam U,

The debug signals are multiplexed with general purpose I/O pins, so some signals will require proper biasing to select the operating mode.

And the JTAG_TMS signal on PTA3 requires a strong pullup resistor for mode selection.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,858件の閲覧回数
puspamnayak
Contributor III

Hi Jeremyzhou,

Thanks for giving technical  clarification.

Have a nice day !

Thanks once again

Regards,

Puspam

0 件の賞賛
返信