Reading the DEFLASH on K40.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reading the DEFLASH on K40.

ソリューションへジャンプ
3,633件の閲覧回数
srinivasanganji
Contributor II

I am using a K40 Kinetis chip. I am trying to read from the DEFLASH. I am using the READ8 macro supplied by Freescale after I do a FlashInit(...).

I get a hard fault exception.

ラベル(1)
1 解決策
3,534件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi

Thanks for the information!! I have implemented your code on my TWR-K40X256 which has a PK40X256VMD100 mounted. The code runs well on my side, so I think maybe your issue is a code issue, please try the attached project and kindly let me know if the problem is still there.

1.PNG

Hope that helps,

B.R

Kan

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
3,534件の閲覧回数
Monica
Senior Contributor III

Hello Srinivasan,

how's the project going? Any breakthroughs?

Please keep us posted :smileywink:

Best regards,

Monica.

0 件の賞賛
返信
3,534件の閲覧回数
srinivasanganji
Contributor II

Well it's going on fine. I am able to read and write to the DEFLASH.

Thank You.

Regards

GRS

(G.R.Srinivasan

Cascademic Solutions Ltd.)

3,534件の閲覧回数
Monica
Senior Contributor III

Great!

0 件の賞賛
返信
3,534件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi,

Would you please provide information about the part number of the K40 device? if you could give a code snippet regarding READ8 issue, that would be better.

Thanks for your patience!!

B.R

Kan

0 件の賞賛
返信
3,534件の閲覧回数
srinivasanganji
Contributor II

FYI

Regards

Srinivasan Ganjigunte

Cascademic Solutions pvt. ltd.

0 件の賞賛
返信
3,535件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi

Thanks for the information!! I have implemented your code on my TWR-K40X256 which has a PK40X256VMD100 mounted. The code runs well on my side, so I think maybe your issue is a code issue, please try the attached project and kindly let me know if the problem is still there.

1.PNG

Hope that helps,

B.R

Kan

0 件の賞賛
返信
3,533件の閲覧回数
srinivasanganji
Contributor II

Thanks Kan. The part # is: PK40X256VLQ100. The READ8 macro is defined in the Freescale file

SSD_FTFx_Common.h as:

#define READ8(address)             

((UINT8)(*(VUINT8*)(address)))

I do a FlashInit(... ) which returns no error. After that I try to read the D-Flash at the base (
#define FLASH_BLOCK1_BASE   0x10000000   // Data flash - NVM


0 件の賞賛
返信