Hi,
i have nearly the same problem as ride. I want to use the MK20DX256VMC7 (MAPBGA, 121 pin) in CodeWarrior 10.3, but this variant is also unavailable in Processor Expert.
Which variant would be the closest fit?
Is there any way to add support manually for CodeWarrior?
Are there any plans to add 121-MAPBGA packages in the next MCUs Driver Suite for Processor Expert?
Thanks in advance.
Hi Jim, i started a new discussion in the PE forum. Sure the package had a great influence on code generation, because the available variants have less pins than 121.