Quick questions about TSS proximity

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Quick questions about TSS proximity

Jump to solution
4,438 Views
kazola
Contributor III

Good afternoon,

I'm using the TSI for a KL05Z. My system is working quite well and I think I know which parameters affect me and which not. However, I would like to ask several questions in order to have some concepts for sure :smileyhappy: All of them are regarding the proximity feature of the TSS library. I also use Processor Expert and FreeMaster. This way of debugging is very graphical and useful :smileyhappy:


My system is very close to an electric line so AC interferences are clearly visible on FreeMaster once I turn on the load. Thus, to begin with, my questions come next, all of them are very easy and / or provide the answer themselves.

     1) I use AFID mode because of the present noise. However, I do not see much difference by tweaking the SLOW and FAST filter values. Are they really worth tweaking in this proximity case? Perhaps they are only useful for touch purposes?

     2) Same question for "Automatic Sensitivity Calibration" and "Baseline Initialization". Do they affect proximity? I think not since I expressly indicate my desidered value in "Proximity & Low-Power Electrode Sensitivity".

     3) I increase the "Response Time" in order to try to be less prone to interferences. However, this is increasing my system's delay also to real proximity events. Do I understand right? :smileyhappy: I cannot increase my sample number because of other reasons and I know "Response Time" is a multiplication factor of "Sample number" (or at least this is what I understood).

     4) Also, I would like to know, more or less, the equivalent time in milliseconds of a Slow DC Tracker Factor = 30 multiplied by a DC Tracker Factor = 30.

     5) Finally, which is the approximate range I could obtain from one square inch of metal? :smileyhappy:

Well, let me know what you think about my questions! :smileyhappy: Happy new year!

Labels (1)
0 Kudos
Reply
1 Solution
4,076 Views
kazola
Contributor III

Hi,

obviously, after 2 months I have managed to do this by myself.

Very poor support from Freescale, which simply cannot be compared to forums from other manufacturers.

Bye.

View solution in original post

0 Kudos
Reply
5 Replies
4,076 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

About TSS library OnProximity feature detailed info, I need to check with related engineer.

I will let you know when there with any feedback.

Thank you for the patience.

best regards,

Ma Hui

0 Kudos
Reply
4,076 Views
kazola
Contributor III

Is there any answer to this question Hui_Ma?

Thanks.

0 Kudos
Reply
4,076 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

I am still waiting for the TSS engineer feedback.

I will let you know when there with any feedback.

Thank you for the patience.

0 Kudos
Reply
4,077 Views
kazola
Contributor III

Hi,

obviously, after 2 months I have managed to do this by myself.

Very poor support from Freescale, which simply cannot be compared to forums from other manufacturers.

Bye.

0 Kudos
Reply
4,076 Views
kazola
Contributor III

Hi Hui_Ma,

that is nice. No problem, I will wait your answer since I'm constantly checking this thread :smileyhappy:

0 Kudos
Reply