Question about switching to VLPR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about switching to VLPR

1,424 Views
vt100
Contributor I

According to the K70 User Manual, when switching to VLPR there is a delay between setting the RUNM field in SMC_PMCTRL and completing the transition to VLPR.
How will the K70 behave if an attempt to switch to WAIT mode occurs during this delay?
Will the K70 switch to WAIT mode, VLPW mode, or is the behavior undefined?

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

1,288 Views
jeremyzhou
NXP Employee
NXP Employee

Hi

Thank you very much for your focus on Freescale Kinetis product.

The datasheet also hasn't illustrated the result happen when execute the enter WAIT mode during entering the VLPR mode.

And I'd highly recommend that avoid the this execution.

Hope it helps,
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply