Problem to debug/run in KL46Z with CodeWarrior

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem to debug/run in KL46Z with CodeWarrior

4,319件の閲覧回数
osvaldoestrada
Contributor I

When I try to debug or run in my board KL46Z, codewarrior show a message:

An error occurred while connecting to the interface hardware or target specified in the Launch Configuration Dialog. For this launch, you may retry/re-specify the connection with the following parameters:

I read that this appear when codewarrior dont recognize the board, but in my case, in the window device shows OpenSDA KL46Z, I tried to put again the DEBUG-APP_Pemicro_v106.SDA file in mode Bootloader but when I try to debug the error appear again.

Thanks for your help.

3 返答(返信)

2,855件の閲覧回数
hectorsanchez
Contributor IV

Hi Luis,

You need to download and install the P&E drivers, you can find them in this website:

P&E Microcomputer Systems

And download the Windows/Linux drivers

Also, this article can help you:

The Freescale OpenSDA Trap: “No Device Available”, or something like that…. | MCU on Eclipse

Keep me informed if this helped you

Best regards,

Héctor Sánchez

2,855件の閲覧回数
osvaldoestrada
Contributor I

Hi Hector

     That dosen´t work, when I try to run or debug the P&E Connection Assistant shows a window like this.

Error.PNG.png

The Codewarrior detect my device but I can´t continue with my debug.

Thanks.

0 件の賞賛
返信

2,855件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Can you check the debugger settings that you are using SWD (and not JTAG)?

pastedImage_0.png

Erich

0 件の賞賛
返信