Problem loading loadbin to NXP FRDM-K66F using SeggerJlink ("Failed to read back RAMCODE for verification")

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem loading loadbin to NXP FRDM-K66F using SeggerJlink ("Failed to read back RAMCODE for verification")

2,805件の閲覧回数
shanker424
Contributor II

Hello, 

My FRDM-K66F board got bricked and I have a problem trying to reprogram the bootloader using Segger J-Link.
the bootloader openSDA v2.2 is downloaded from  openSDA 2.2 and the following method is used to load the bootloader

fol.PNG

I am using Segger J-Link Commander for flashing the bootloader, When I attempt to load the bin file I get the following error message  "Failed to read back RAMCODE for verification" from JLink Commander.

error.PNG

Can anyone help? Thanks in Advance.

2 返答(返信)

2,391件の閲覧回数
r14713
NXP Employee
NXP Employee

Hello,

Looks like you are trying to flash the bootloader image to the K66 and not the K20  (where you need to flash it)

To connect the J-Link to the K20  you can access through the "OpenSDAv2 debug" header.

See page 4 of:

https://www.nxp.com/docs/en/user-guide/FRDMK66FUG.pdf

The 2 headers are similar.  1 is for the K20, the other for K66.

Regards

2,391件の閲覧回数
shanker424
Contributor II

Thanks Gary Anderson, it's working.

0 件の賞賛
返信