Power K64F with external power supply

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Power K64F with external power supply

4,508 Views
fahimrahman
Contributor I

I've got a FRDM-K64F that I want to power up using an external power source. I put 5V through V_in (pin 16) and the connected the ground to my voltage regulator. I can see the Ethernet light turn on, indicating there is some power going through, but the main 'on' light isn't on, and nothing happens when I press the 'reset' button.

To double check that is meant to work, I connected it to my PC using the USB, hit 'reset', and it worked fine.

How can I run this with an external power supply?

Thanks!

Labels (1)
Tags (2)
0 Kudos
Reply
6 Replies

3,520 Views
michaelkoller
Contributor III

Hey there!

I have run into the same problem as OP and I have tried two things.

I tried my power supply Voltcraft VLP-1405 with 5V and I have tried the 5V which are supplied from a DC/DC stepdown converter, that I ultimately want to use.

There is only the red light on, as the OP reported, not the green one.

Which steps can I take to avoid this?

Also, if this I should not revive this thread, please tell me so I can open a new one.

Cheers,

Michael

0 Kudos
Reply

3,520 Views
maksim_lipskiy
Contributor III

H.!
I made a smooth flow of power to the power was set for 100 milliseconds.

0 Kudos
Reply

3,520 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Fahim,

Before I answer your question, I'd like to check with you about whether you connected the external 5V supply to VDD pin directly or not.

2015-06-23_9-54-57.jpg


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,520 Views
fahimrahman
Contributor I

I believe so, yes. 5V to pin 16, ground to pin 14.


IMG_20150623_082808.jpg

0 Kudos
Reply

3,520 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Hi Fahim,

I've reproduce your procedure to supply the board from a external 5 voltage, however the board can work well, as the Fig 1 illustrates.

IMG_20150624_095151.jpg

                                                                            Fig 1


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,520 Views
maksim_lipskiy
Contributor III

Your DC power very long risetime (for example  DC-HY5002 about 400 ms). Therefore, the board is working.
If you are using a power supply unit SPS-026-05, the board will not work. Because risetime very small.

0 Kudos
Reply