Possible errata on KL25 Reference Manual

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Possible errata on KL25 Reference Manual

Jump to solution
3,534 Views
danielcolon
Contributor II

Hello".

I've been trying to configure the PIT Module changing the registers manually following the KL25 Reference Manual (KL25P80M48SF0) it didn't work, so I look at the code in Kinetis SDK and I realize the bits numbers on the Reference Manual tables were backwards. I mean, the bit 0 appears as bit 31 on the Reference Manual.

After configuring the registers with bits as they should be, the PIT module works fine.

Is the Reference Manual wrong? or I missed some note that indicates this backwards convention?

Note: I don't sure if this question goes here.

0 Kudos
Reply
1 Solution
3,366 Views
mjbcswitzerland
Specialist V

Hi

All of the PIT registers in the KL25 user manual are numbered incorrectly.
They should count 31...0 rather than 0...31.

As far as I am aware this error is limited to the PIT section of only that manual - all other manuals seem to have it correct.

Regards

Mark

View solution in original post

0 Kudos
Reply
4 Replies
3,366 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Sorry for the inconvenience. I have report this issue to our document team.

Best Regards,

Robin

0 Kudos
Reply
3,367 Views
mjbcswitzerland
Specialist V

Hi

All of the PIT registers in the KL25 user manual are numbered incorrectly.
They should count 31...0 rather than 0...31.

As far as I am aware this error is limited to the PIT section of only that manual - all other manuals seem to have it correct.

Regards

Mark

0 Kudos
Reply
3,366 Views
danielcolon
Contributor II

Thank You!

Wich other manuals do you know about the KL25Z?

Regards.

Daniel.

0 Kudos
Reply
3,366 Views
mjbcswitzerland
Specialist V

Daniel

I meant all other manuals to other parts (eg. KL26, KL27 etc.).

Regards

Mark

0 Kudos
Reply