Porting KINETIS512_SC sample code to Kineties K60FX512 series

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Porting KINETIS512_SC sample code to Kineties K60FX512 series

1,634件の閲覧回数
mithunp_s
Contributor III

Dear All,

My customer is working on MK60FX512,, I downloaded  KINETIS512_SC sample code but I notice these are written to K60DN512 please help me how can I make them useful for  Kineties K60FX512 series

Regards

Mithun

ラベル(1)
0 件の賞賛
返信
1 返信

1,313件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Mithun P:

There are already some sample codes in other package called KINETIS_120MHz_SC, which contains applications for K60FX512. You can download it from the next link:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=K60_120&nodeId=01624698C9DE2DDDAF&fps...

Hope this is useful!

/Jorge Gonzalez

0 件の賞賛
返信