Porting KBOOT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Porting KBOOT

2,629 Views
jorgehoraciogon
Contributor II

Hello everyone! I need to port the kinetis bootloader to the MK53DN512CMD10 uC, the document "Kinetis Bootloader v2.0.0 Reference Manual" that I´m using indicate to me I need a header from the webpage of NXP, but actually that header does not appear. Somebody could tell me if that file exist? (MK53DN512CMD10.h)

I would be very thankful for your answer.

0 Kudos
Reply
1 Reply

2,559 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,

The MK53DN512CMD10.h is the previous kind of head version, please choose the MK53DZ10.h which support the K50_100 series MCU.

Hope it helps.


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply